Twitter Facebook Linkedin Youtube
Prysmian Group UK

UK

Prysmian group - logo

Prysmian - Draka - logo

Link Boxes

Link Boxes

An underground link-disconnecting box is a low voltage cable joint that incorporates a removable link such that it may be “switched”. Increasing pressure on the electricity supply companies to reduce customer interruptions means that link boxes are used within the distribution network to increase its flexibility as different parts of the networks can be energised or de-energised as required. The link box also has the facility to connect localised customers directly via a generator. Also during maintenance or a repair the solid links can be replaced with fused links.